Skip to main content
Cart
Posted by Engineering Centre Team10 months ago

Volatile Organic Compound testing and why testing is important

Firestop,Sustainability,VOC

838

Introduction
Firestop products have a broad selection of tests and certification providing data on the environmental and health impact of products. VOC test certificates provide evidence that products meet nationally and internationally defined and recognised standards for VOC Emissions and Content. When selecting a product for an application or project, VOC certification supports both the achievement of Green Building Certification and project specific sustainability goals and helps in the selection of the product.

VOC Definition
VOC stands for Volatile Organic Compound. VOCs are chemicals that easily become vapors or gases at room temperature. These include carbon based organic materials such as alcohols, aldehydes, organic acids amongst many others. When a wet applied chemical product cures (for example a foam) or dries (such as a sealant), VOCs that are not fully reacted or embedded into the chemical product can evaporate into the air.
This so-called off-gassing can happen immediately during application impacting the construction worker or over time impacting the health and safety of building occupants. VOC exposure can lead to unpleasant symptoms such as headaches, eye, nose or throat irritation, dizziness, nauseous, difficulty to concentrate and sensitivity to odours. Some VOCs are carcinogenic.
By carrying out VOC testing on products at ISO 17025 Accredited Laboratories, Hilti provides its’ customers the transparency for product choice based on internationally recognized standards.

Green Building Schemes and VOCs
Numerous Green Building Schemes such as LEED, BREEAM, WELL, DGNB and Living Building Challenge set out minimum requirements for air quality in buildings. Providing product level certification can help achieve those minimum requirements. VOC requirements are outlined for Adhesives, Sealants, Paints and Coatings as well as thermal insulation products with, in some cases, such as BREEAM, specific limits set out in the Green Building Scheme. Firestop Product level VOC Certificates can support achievement of credit points in those Green Building Schemes with LEED and BREEAM specific attestations available for certain products, leading to whole building certification.
Table 1 below summarises the types of test attestations available for Firestop products and which Green Buildings Schemes they can support achievement of credits.


Table 1: Certificates and Green Building Scheme Relevance

Conclusion
Environmental Scheme Support is part of Hilti's Sustainability Strategy. This is why VOC tests have been carried out and certificates are available for most of Hilti's Firestop Products, ensuring that all new products fulfil the test requirements in the relevant markets and countries and that existing products are re-tested at regular intervals to ensure continued fulfillment of the standards.
VOC Certificates for Firestop support achievement of credits in Green Building Schemes and in doing so supports Hilti's Sustainability Strategy: to be our Customer's Best Partner for Sustainability.

Further Information
To find the VOC certificates, please check the Product page on Hilti Online under Sustainability Documents. Read more about the Sustainability at Hilti under www.hilti.group/content/hilti/CP/XX/en/company/Sustainability/Sustainability.html

References:
LEED 5.0 Building Design and Construction April 2025, Launch Edition
LEED V4.1 Building Design and Construction October 2021
LEED V5.0 Rating System Building Design and Construction: New Construction Core and Shell
BREEAM-NOR v6.0 New Construction Technical Manual SD5076NOR
BREEAM International New Construction Version 6.0 Technical Manual-SD 250
DGNB System ENV1.2 Risiken für die lokalen Umwelt
WELL v2 International WELL Building Institute.
Living Building Challenge 4.1 Program Manual, A Visionary Path to a Regenerative Future October 2024
Hilti Sustainability Strategy

No comments yet

Be the first to comment on this article!