Skip to main content
Cart
Posted by Hilti BU Anchorsover 1 year ago

White Paper presented by Hilti and NewCivilEngineer

anchor design,Profis Engineering,productivity,SBP

1.7K

Designing steel to concrete connections is a key safety-critical task on many construction projects. Yet based on a survery carried out by the NCE, 33% of engineers say optimising connection design is challenging.
In addition to this being a challenging task, 10% of engineers have expressed that this normally takes more than 8 hours to design connections.

In 2019 we saw the launch of our new PROFIS Engineering anchor design software that will solve some of these challenges. Not only this allows you to design to the most up to date codes EC2 EN1992-4 but it also can save up to 50% in time by doing the checks with one piece of software on both the baseplate and the anchor.

Have a look into the White Paper article we presented with the NCE to gain a better insight into the full article clicking here

If you would like to start using PROFIS Engineering and start design as per EC2 visit our webpage clicking here

You are also welcome to ask us for support: simply leave a comment or post your question in the community, or improve your knowledge and skills via our Webinars or training sessions.

For the latest news in engineering solutions and innovations follow us on: LinkedIn, Instagram and Twitter


To view further articles on PROFIS Engineering please click here


No comments yet

Be the first to comment on this article!