Skip to main content
Cart
9 months ago

EPD's and life cycle assessments in passive fire protection

EPD,LEED

962

Introduction
Environmental Product Declarations (EPDs) and Product Life Cycle Assessments (LCAs) help achieve credits in Green Building Schemes aswell as providing Data Transparency on the CO2 impact of a product. Many different construction projects, including Energy, Industry, Commercial or Residential are Green Building Certified or have their own Sustainability Targets. Firestop products with EPDs or Life Cycle Assessments help to achieve project sustainability goals whether supporting credit achievement in Green Building Certification, in calculating the CO2 impact of a building or in the selection of products to achieve CO2 targets.

This goal of this article is to explain the fundamentals of Environmental Product Declarations and Life Cycle Assessments and how they can add value to your project.

Difference Between Life Cycle Assessments and EPDs
The carbon footprint of any product can be measured using two standardised calculations: a Lifecycle Assessment (LCA) and Environmental Product Declaration (EPD). Both itemise a product’s environmental impact according to the stages listed below, but vary in precision. LCAs can rely on averages, whereas EPDs require real energy data from the factory and verification by a certified external verifier.

Life Cycle Stages
The Life Cycle Assessment is calculated based on the environmental impacts across the entire Life Cycle of the product shown in Figure 1.

The Life Cycle is split up into categories from A-D. The impact of each stage is calculated and sums up to the final overall impact measured in kg CO2 / 100 years.

Apart from the kg CO2 calculated, a number of other impact categories are assessed. These are visible on the EPD and include amongst others Ozone Depletion Potential, water use, acidification potential. The EPD can be a useful source of information beyond CO2 when assessing the environmental impact of a product.

Figure 1: Life Cycle Stages

Environmental Product Declarations
Environmental Product Declarations set out the environmental impact of a product from Raw Material and Manufacturing to Removal from the Building to Product End of Life. (see figure 1 above). The calculation is based on real energy data from the factory and is third party verified by an external verifier. The environmental impact is calculated based on kg equivalents of CO2 Emissions/kg product. The assessment from Cradle to Grave is called a Life Cycle Assessment and considers all aspects related to the product manufacturing, use and end of life, including raw material impact, manufacturing energy, manufacturing and product waste, transport to the jobsite, removal from the building and end of life scenarios such as recycling, incineration with / without energy recovery or landfill. It also provides information on how and where the product is manufactured, if recycled / recyclable or biogenic (e.g. biobased, wood) materials are included and if the product contains REACH restricted / Substances of Very High Concern.

In passive fire protection, generally the biggest contributing factor is raw material extraction and chemical manufacture. The in-use phase generally has a negligible impact, since once the product is assembled in the building it will stay there until the building end-of-life. The end-of-life scenario depends on the product type, how easy it is to remove from the building and recyclability.

The CO2 footprint is calculated based on 1kg of product. This information enables calculation of the total CO2 footprint product used in the application or to simply have an indication of the environmental impact of the product.
There are many other environmental indicators covered in EPDs which can give insights into how the product impacts the environment. The CO2 value provides an overarching indicator of the product’s environmental impact.

Life Cycle Assessments
Life Cycle Assessments also set out the environmental impact of a product from Raw Material to end of life however are generally based on average energy data from the factory and provide the results for 1 unit of product as sold. They are not third party verified however still provide an insight into the Carbon Footprint of a product.

EPDs, LCAs and Green Building Schemes.
Green Building Schemes such as LEED, DGNB and BREEAM have specific criteria for materials and the Life Cycle Impact of Buildings. Whole buildings or projects are certified based on detailed criteria in those Green Building Schemes. Table 1 shows examples of Green Building Schemes and the credit categories where EPDs can support the achievement of points. If a project is certified under any of these schemes, a product level 3rd party verified EPD can be a big help in achievement of credits towards the overall Building Certification. In LEED certified projects, critically reviewed LCAs can also contribute to credits however have a lower credit contribution compared with third party verified EPDs.

EPDs, LCAs and Project Sustainability Goals
If your project has specific goals for CO2, a Product EPD and an LCA provides the data transparency needed on the CO2 impact of the Firestopping used in the application with the differences in data outlined above.


Table 1: Green Building Scheme and Credit Category with Environmental Product Declarations Relevance.
*certificates contribute towards achievement of points in whole building assessment. For details of credit calculation, see related Green Building Scheme (please see references),

Hilti Sustainability Strategy and SBTi
To support Climate Goals and Reduce Global CO2 Emissions due to the built environment, Hilti has set ambitious reduction targets until 2032 validated by the Science Based Targets Initiative with the long-term goal to achieve net-zero Emissions by 2050. One main contribution to achieve that is making products more Sustainable.

Hilti’s ambition is to become our customer’s Best Partner for Sustainability both through the solutions we offer and how we operate and is based on the 3 strategic pillars of Environment, People and Society. The Environment Pillar includes Decarbonisation of own operations, more sustainable products and more sustainable construction. EPDs, providing third party verified Data Transparency on CO2, are a key part of this Strategy.

Hilti Passive Fire protection
Today, Hilti Firestop Products can support Hilti Customers and Building Owners in the selection of Supplied Products with the provision of Environmental Product Declarations and critically reviewed LCAs. These are available for several different pre-formed and wet applied products including Speed Sleeves, Blocks/Plugs, Cast-In Devices, Firestop Foams, Steel Coatings, Adhesives and Sealants and Cavity Barriers.

Beyond firestop, Hilti offers over 50 EPDs covering over 1000 items including anchors and MEP supports.

Summary and Conclusions
Both LCAs and EPDs Provide Data Transparency on Product Carbon Footprint – kgCO2e / kg product, Information on the product, the manufacturing process and location as well as raw materials used and in doing so help achieve credits in Green Building Schemes.

The main difference between the two is use of real plant data collected over 1 calendar year (EPDs) versus generic data (LCAs).
In addition, EPDs are generally third party verified whereas LCAs are not.

They support Construction Projects on the assessment and achievement of sustainability goals and enable calculation of the whole building / project CO2 footprint, provide transparency on other environmental impact categories such as Ozone Depletion Potential, Water Use, Depletion potential of the stratospheric ozone layer (ODP), water usage and Eutrophication Potential and with Third Party Verification, the calculation and data has been critically reviewed and verified by an external assessor.

To access all EPDs available, check Hilti Online on the product page under Sustainability.

References:

LEED 5.0 Building Design and Construction April 2025, Launch Edition
LEED V4.1 Building Design and Construction October 2021
BREEAM-NOR v6.0 New Construction Technical Manual SD5076NOR
BREEAM International New Construction Version 6.0 Technical Manual-SD 250
DGNB System Kriterienkatalog Gebäude Neubau Version 2018
Financing Transformation A Guide to Green Building for Green Bonds and Green Loans 2024
Alliance HQE, Bre, Green Building Council Australia, Singapore Green Building Council, U.S. Green Building Council USGBC
Hilti Sustainability Strategy

No comments yet

Be the first to comment on this article!