- Home
- Buying Guide for Power Tools and Inserts
- Impact & Torque Wrench Products - A Quick Guide | Hilti UK

Choose the right Torque Wrench for your needs
A torque wrench, impact torque wrench or ratchet, is an essential tool for anyone working on projects that require precise tightening of fasteners, from automotive repairs to construction tasks. Over-tightening or under-tightening bolts and nuts can lead to damaged parts or dangerous conditions, which is why choosing the right torque wrench is crucial. This guide will walk you through everything you need to consider when selecting the best torque wrench for your needs.
What is a Torque Wrench?
A torque wrench is a specialized tool used to apply a specific amount of torque to a fastener. Torque is the force applied to rotate an object, such as a bolt or a nut. Torque wrenches are designed to prevent over-tightening or under-tightening, which can be critical in applications like automotive repairs, where incorrect torque can cause components to fail.
There are various types of torque wrenches available, each with its strengths and ideal applications. Selecting the right one depends on your specific needs, the types of projects you’re working on, and the precision required.
Types of Torque Wrenches
Before choosing a torque wrench, it's important to understand the different types available and their uses. Here are the most common types:
1. Beam Torque Wrench
The beam torque wrench is the simplest and most affordable type. It consists of a long, flat bar (the beam) and a smaller, pointer bar that deflects as you apply torque. The pointer moves along a scale on the handle, showing how much torque is being applied.
- Advantages: Cost-effective, simple to use, and does not require recalibration.
- Disadvantages: Less precise than other torque wrenches, harder to read accurately in low-light or awkward positions.
2. Click Torque Wrench
The click torque wrench is the most popular type for users of all kinds. It emits an audible “click” when the preset torque is reached, making it easier to use compared to beam wrenches.
- Advantages: Accurate, easy to use, and suitable for a wide range of applications.
- Disadvantages: Requires periodic recalibration and is typically more expensive than a beam wrench.
3. Digital (Electronic) Torque Wrench
A digital torque wrench offers the most precise control, displaying real-time torque readings on an electronic screen. Many models even have features like memory storage and alerts when you've reached the target torque.
- Advantages: Extremely accurate, easy to read, and often feature-rich.
- Disadvantages: Expensive, requires batteries, and periodic recalibration.
4. Dial Torque Wrench
A dial torque wrench has a dial gauge that shows the torque being applied. It's very accurate and often used in industries that require high precision.
- Advantages: High accuracy, especially useful for quality control and specialized industries.
- Disadvantages: Expensive depending on user options.
5. Split Beam Torque Wrench
Similar to click wrenches, the split beam torque wrench doesn’t require as frequent recalibration, which makes it a good choice for professionals who use them regularly. They are durable and reliable but generally more expensive.
- Advantages: Reliable, less frequent recalibration needed, durable.
- Disadvantages: More expensive, usually bigger vs click wrenches.
6.Cordless Impact Torque Wrench
Impact torque wrenches are specialized tools that combine the high-torque output of impact mechanisms with the precision of torque wrenches. They deliver powerful bursts of torque, allowing users to achieve the desired torque level quickly and efficiently.
- Advantages: Precision and great for quick tightening or loosening of bolts.
- Disadvantages: Higher maintenance costs and more expensive vs manual torque tools.
Key Considerations for Choosing a Torque Wrench
1.Torque Range
The most important factor is the torque range you need for your project. Torque wrenches are rated to work within a specific torque range, typically measured in Newton meters (Nm) or foot-pounds (ft-lb). Check the specifications for the fasteners you will be working with to ensure the wrench you choose can apply the appropriate torque.
For example:
- Automotive lug nuts generally require 80-100 ft-lbs of torque.
- Bicycle components might need anywhere from 4-10 Nm.
2. Size and Drive
Torque wrenches come in various sizes and drive types, which determine how well the tool fits into your working space and matches your fasteners. The most common drive sizes are:
- 3/8-inch: These wrenches are generally compact and easy to use in extremely tight spaces
- 1/2-inch: regarded as the most common size of impact wrench and offers the best balance between precision and power.
- 3/4 inch: The largest, common impact wrench sizes and are best for safely removing large nuts and bolts.
3. Material and Build Quality
Choose a wrench with a sturdy, durable build, as these tools often face heavy use. Look for torque wrenches made from high-grade materials for better longevity. Higher-quality tools will resist wear and tear better, maintaining accuracy over time.
4. Calibration and Maintenance
Click and digital torque wrenches require regular recalibration to ensure accuracy. This can be an additional cost, but it's crucial in maintaining tool performance. Some manufacturers provide calibration certificates with the tool, which can be important for professionals who need accountability. Beam wrenches, on the other hand, don’t need recalibration as they don’t have internal mechanisms that can wear down.
5. Comfort and Ergonomics
Since you’ll be using your torque wrench repeatedly, comfort is an important factor. Look for tools with ergonomic handles that reduce strain on your hands and wrists. Selected digital models also offer reduced vibration or high vibration alerts, adding to ease of use.