- Home
- Buying Guide for Power Tools and Inserts
- Angle Grinder Buying Guide

Angle Grinder Buying Guide
Choose the right tool for your needs
An angle grinder is an essential power tool for any professional trade on site.
However, with so many variants available to buy, choosing the right one for your needs can be overwhelming. As a versatile tool that can cut, polish and grind across a variety of materials, it’s no wonder that an angle grinder is a must-have tool for a range of projects.
Our slimmed-down guide will look at the various options to help you navigate and choose the best angle grinder for your needs.
What to Consider When Buying an Angle Grinder
Disc size
Angle grinders can accommodate a variety of different sized blades which are used for different applications. While the 125mm disc is the most common, other sizes are available including:
- 115mm / 4.5 inch disc - ideal for tasks that require manoeuvrability, with the need for accuracy and precision
- 125mm / 5 inch disc – can be used for regular grinding, cutting, sanding etc., can handle regular and heavy jobs based on power and performance of the grinder
- 150mm / 6 inch disc – similar performance to 125mm discs, while being able to handle some heavier tasks
- 230mm / 9 inch disc – for heavy duty tasks like cutting slabs. They operate slower, but can also be used for sanding or polishing
Power options
In terms of power supply, angle grinders are usually available in one of two power options:
Corded Angle Grinders
- Uses mains electricity
- Delivers constant power output
- Ideal for tasks that need continuous power
Cordless Angle Grinders
- Uses rechargeable batteries, such as our 22v Nuron Battery (or other 18/20v option)
- Offers convenience for working anywhere without needing power cables
- Ideal for jobs that require high levels of mobility
Wattage and voltage
Generally speaking, grinders with larger discs will need more power. However, the specific application will also dictate the number of watts used.
A grinder with variable speed could use differing amounts of watts depending on the speed and application. Devices will range from 500w to 2400w and more.
In terms of voltage, many brands offer corded products, as well as battery chargers for cordless products, in either 110v or 230v models.
While this doesn’t affect the performance of the products, its main benefit is that of safety, with 110v offering less risk to users on site in the event of a shock.
Ergonomics and comfort
Angle grinders are often used for small and heavy-duty tasks. So useability from a comfort and ergonomics perspective is a big factor that shouldn’t be overlooked. This is also more important to consider if you’re going to be using a grinder for prolonged periods and frequency.
The key factors to consider for this are:
- Weight and balance: Lighter weight angle grinder models can reduce user fatigue
- Handle design: Ergonomic and anti-vibration handles improve comfort, control and safety
- Size: Compact tools can be easier to work with and offer better control
Speed (RPM)
Many grinders can operate within a certain speed range of rpm (rotations per minute) for the discs they use. Some start from 3000rpm, with models in the market available up to 12,000rpm or more.
While higher speeds are suitable for cutting and grinding harder materials, lower speeds provide more control for delicate and considered tasks like polishing. You’ll also find that many models offer adjustable speed controls, making them an all-rounder for applications across the job site.
Just remember, different tasks require different speeds and blades from your angle grinder – so a variable speed tool is a bonus across applications and materials.
Safety features
As with any tool that’s capable of cutting and grinding, care should be taken when using an angle grinder. Most come with similar features from nearly all leading manufacturers.
- Blade guard: Almost standard on most angle grinders, protects you from sparks and debris
- Dust port option for accessories: Dust ports are available on selected grinders, such as those for concrete, which can be connected to a vacuum. Though many grinders won’t have this as an option.
- Quick disc brake: Stops the disc quickly within a few seconds after operation
- Kickback prevention: Stops the tool if the disc gets jammed on the material surface – known as Active Torque Control (ATC) on Hilti products
- Dead man’s switch: Button that requires continuous pressure to operate, turns off when button is released
- Overheating protection: Stops the tool operating if it is too hot, will only operate again once cooled down
Don’t forget, additional safety should be considered when using an angle grinder, including dust mask, earplugs, safety goggles and gloves.
Motor type: Brushless Motor vs Carbon Brushes
Many earlier tools and products, including power tools, kitchen products and washing machines, used carbon brushes as a way to transfer power from a stationary part of a motor to a moving component in order to operate. These would need constant contact between two surfaces, and over time, grind or wear down. In addition, when it comes to an efficient motor in an angle grinder, friction and heat ideally needs to minimised. As technology has developed, manufacturers have switched to using magnets and/ or a type of inverter to do the same job, without the need for contact in the motor or internal parts. These are known as brushless motors, which means that the motor could potentially last longer
However, as the build components for a brushless motor are normally more sophisticated than their carbon brush counterparts, there is a higher cost to pay for products with a brushless motor. But what you do get, is a tool that can last longer. So while a motor with carbon brushes may be cheaper, it may not last as long as you need it – or it may need to be repaired more often.
Angle Grinder Discs
There are different types of inserts you can use with an angle grinder. Here are some of the most common types you need to consider for a range of applications.
Cutting discs
One of the most common types of discs used with an angle grinder. Different discs ore optimised for use in specific materials. Abrasives - Hilti United Kingdom
Diamond blades
Often used by different trades for heavy-duty cutting through a variety of materials including PVC, metals and natural stone. Diamond blades and cup wheels - Hilti United Kingdom
Fibre discs
These are usually made with abrasive ceramic grains and are commonly used for rough to fine grinding of stainless steel and other materials. Abrasives - Hilti United Kingdom
Non-woven discs
Primarily used for finishing on steel. Some discs may require an additional backing pad for use with the disc itself. Abrasives - Hilti United Kingdom
Grinding discs
Can be used for preparation of metals and/or removing the top layer of metal surfaces through abrasive grinding. Abrasives - Hilti United Kingdom
Mortar Rake discs
Used by pointing specialists and general contractors to remove old or unwanted mortar from surfaces - such as the SPX Tuck Point diamond blade. Diamond blades and cup wheels - Hilti United Kingdom
Flap discs
For rough to fine grinding of stainless steel. Can be used on other material surfaces. Examples include our AF-D FT SPX Flap Disc AF-D FT SPX Flap disc - Abrasives - Hilti GB[DM1]
You can view the full range of discs on our dedicated abrasive page and diamond blades/ Cup Wheel page.
Abrasives Abrasives - Hilti United Kingdom
Diamond Blades and Cup Wheels Diamond blades and cup wheels - Hilti United Kingdom
Angle grinder maintenance
To prolong the life of your grinder, we recommend regular servicing and maintenance. Angle grinders are often used in environments where there is dust and debris – often produced when using the grinder itself. In addition, especially with regular heavy-duty use, they may need repairs. It’s worth choosing a tool or brand which offers repair and maintenance services to ensure your grinder works as it should.
Hilti offers an online repair service where users can log a repair within minutes. In addition, if you choose to lease your tools from us, you can take advantage of free repairs and maintenance to keep your tools going for longer – we’ll even provide you with a loan tool so you can keep on working while your tool is with us.
Browse the right tool for your needs
Choosing the right angle grinder depends on your specific needs, including the type of project you’re on, materials, and the preferred power source. By considering factors like disc size, working material, tool type and more, you can find a tool that suits your project and long-term demands.
Most professionals in the trade will choose a grinder based on its features, such as a dead man’s switch, brushless motor or disc size, and the applications it will be used for. For those who need constant power over a prolonged period, such as those in a workshop, yard or site, a corded grinder may be the best option. But if you need the freedom of movement and are hopping from task to task, without the inconvenience and risk of power cords, then the corded option is probably what you need.
Use the filters on our dedicated pages to find a product for your needs.
Grinders and sanders Grinders and sanders - Hilti United Kingdom
Diamond blades and cup wheels Diamond blades and cup wheels - Hilti United Kingdom