- Home
- Solutions
- News and Events
- Hilti Blog
- Getting your lighting right this Christmas
5 min. read, Dec. 2024
Getting your lighting right this Christmas
May your job site be merry and bright
Nothing makes it feel more like Christmas than the lights. Candles on the mantlepiece and a roaring fire underneath, a well-dressed tree lit up with fairy lights, houses covered in bright festive decorations, high streets brought to life by cheery displays – and if you’re lucky, falling snow framed by the street light’s glow.
As the dark nights draw in earlier and earlier, we need that light, and that’s also true on the job site. Just as important as illuminating your home is making sure your construction site is kept light and bright...
and you can take some inspiration from Santa and his elves to help.
Cordless tower light SL 10-22
Elves work to a strict deadline and can’t afford downtime. No matter how hard it gets, they’ve got millions of presents to get wrapped and loaded onto Santa’s sleigh in time for Christmas.
Our Cordless tower light SL 10-22 helps them keep working no matter how dark it gets. 360-degree coverage and an IP55 rating for outdoor use at dawn, dusk or night time makes it ideal for achieving shadow-free coverage on site.
It’s also easy to set up, has stable footings and can be extended up to a height of 2.1 metres so its light will reach over any passing reindeer – or obstacle on your building site. And when it’s not being used, you can put it to work as a stand-in Christmas tree!
Find out moreSL 4-22 cordless searchlight
Once the presents are wrapped and loaded into the sleigh, it’s delivery time! Santa visits a huge number of houses in a single night, but one thing they all have in common is that they are a hazardous working environment.
Every roof he lands on is dark and slippery. Without some way to see where he’s going and find his way to each chimney safely, Santa could easily hurt himself and Christmas would be ruined!
Luckily, Santa can call on Hilti’s SL 4-22 cordless searchlight for assistance. It has a powerful 1,800 lumen long range beam with three modes – searchlight, floodlight and combined – which ensure Santa can get where he needs to go safely.
It’s also designed for inspecting pipes, ducts, utility and electrical installations which makes it perfect for seeing whether there are any obstructions in the chimney before he heads down.
Find out moreSL 2-22 LED work light
Once he’s inside, Santa has to be quiet and make sure not to wake anyone up. He can’t turn on the big lights in the house, but he needs to put the presents in the perfect place under the tree and double check he’s not delivering to anyone on the naughty list!
The SL 2-22 LED work light is perfect for what he needs. It’s rotating head and large hook are ideal for one-person jobs. He can attach the light to a wide range of objects nearby, such as pipes, ladders, scaffolds and rafters and get even, natural light at three brightness modes.
Even better, the high-output Nuron cordless battery means he will get a full 24-hour charge at full brightness – more than enough to see Santa through the night and make sure he gets all the little details of his work exactly right.
Find out moreSL 6-22 LED construction light
Once his busiest night of the year is complete, Santa flies his sleigh back to the North Pole and there’s only one task left – getting his work site back all packed away safely.
It’s still dark and there’s lots to do, but the SL 6-22 LED construction light offers a simple, versatile lighting solution that makes work on any site easy and safe.
It’s easy to move and can be attached to or hung from a range of surfaces. The light also has a rotating head and can be attached to a tripod if needed. Together, those features guarantee complete coverage of any site, and the Nuron battery system means you can count on 100% brightness for at least a whole day.
Find out moreSo, whatever you’re doing this holiday season, have plenty of fun and follow Santa’s example by keeping your construction sites brightly lit with our range of essential lighting tools!