- Home
- Solutions
- News and Events
- Hilti Blog
- Eco-Friendly Building Materials

10 min. read,October 2024
Eco-Friendly Building Materials
Key Trends for future
The construction industry is changing fast. Sustainability is no longer a buzzword. It’s becoming a legal necessity and a commercial imperative. Eco-friendly building materials, from traditional options like straw and bamboo to innovative solutions like recycled metal and mass timber, are driving this green revolution, offering environmental benefits without compromising quality or functionality.
Mass Timber: A Step Toward Greener Construction
Mass timber construction involves the use of engineered wood products such as cross-laminated timber (CLT), glue-laminated timber (Glulam) and Dowel-laminated timber (DLT). It represents a clear step forward in sustainable building. The life cycle benefits of mass timber, including its ability to sequester carbon and possibilities for recycling, could lead to a significant longer-term reduction in environmental impact if resources are managed properly. In addition, its load-bearing capacities, fire-resistant properties and role in energy-efficient building designs are helping to reshape modern architecture and building practices.
Sustainable Precast Concrete: Rethinking Traditional Practices
Sustainable precast(1) concrete has come a long way. It typically has a low water/cement ratio, excellent insulation and thermal properties, and high energy efficiency. Durability and recyclability also significantly enhance the sustainability credentials of precast concrete. This is further enhanced by the use of local and natural materials such as sand and gravel in its composition. Using these materials not only provides a strong example of environmental stewardship, but also helps to reduce transportation emissions by sourcing materials closer to the construction site.
Several other key innovative technologies and practices have boosted the sustainability credentials of the material, and have improved its functionality and efficiency in construction. These include:
● Building Information Modeling (BIM) [2] : This method streamlines the entire construction process, from design to the construction phase to building operation. BIM software, such as Tekla and BIM 360, supports accurate up-front modeling of precast elements and reduces the risk of ad hoc solutions on site.
● Virtual and augmented reality: These technologies provide accurate, real-time scanning of jobsites, helping to improve project management, communication, and efficiency. The use of virtual and augmented reality reduces the need for constant physical presence on site, allowing remote monitoring and decision-making.
● 3D printing in precast concrete[3] : Used to create precise and reusable forms, this innovation minimises human error and increases manufacturing efficiency.
● Exoskeletons [4]:These wearable devices help reduce muscle fatigue during heavy-duty tasks like tough rebar drilling or while working above shoulder level. They are designed to significantly reduce physical strain and the risk of injury, especially critical when handling heavy precast elements.
● Loader cranes: These facilitate the efficient and safe movement and installation of precast panels, improving overall site safety and logistics.
● Retractable enclosures: These structures create optimal environments for curing and production, helping to maintain consistent quality by controlling external factors such as temperature and humidity.
The Rise of Alternative Materials: Recycled Metal and Bamboo
Recycled metal [5], derived from scrap materials, reduces the need for new metal production, which is typically energy-intensive and polluting. The use of recycled metal helps conserve resources and can also minimise waste and energy consumption. In construction, recycled metals are commonly used for structural framing, roofing and façades due to their durability and strength. However, they may require additional processing to ensure their suitability for specific applications. They are also used in decorative elements and fixtures, providing both functionality and aesthetics.
Meanwhile, bamboo[6] is emerging as a robust, sustainable alternative to traditional hardwoods. Its rapid growth cycle and ability to thrive without pesticides make it an environmentally friendly option. Despite its tensile strength, which is comparable to steel, bamboo faces issues such as susceptibility to moisture and pests if not properly treated. It can be used in a variety of applications, from structural elements to aesthetic finishes, but the need for special treatment and design considerations to mitigate these vulnerabilities can add complexity and cost to projects.
Technological Advances and Eco-Friendly Practices
Structural Insulated Panels (SIPs): Enhancing Energy Efficiency
Structural Insulated Panels (SIPs) [7] [8] typically consist of a layer of foam insulation sandwiched between two structural shells, offer superior energy efficiency compared to traditional framing methods. The airtight nature of SIPs significantly reduces heat loss and gain, improving the thermal performance of buildings. This efficiency translates into lower heating and cooling costs, and can reduce a building's carbon footprint. In addition, the streamlined construction process associated with SIPs reduces waste and shortens project schedules. This is important because shorter construction times mean less on-site energy consumption and fewer emissions from building activities. Faster project completion also minimises disruption to the surrounding environment and reduces the overall environmental footprint of the construction process.
Innovative Insulation Materials: Cellulose and Recycled Denim
The shift toward innovative insulation materials, such as cellulose and recycled denim, reflects a growing awareness of the environmental impact of building materials. Cellulose insulation, made from recycled paper, provides excellent thermal insulation and is fire-resistant, making it a safer, more sustainable choice. In addition, its manufacturing process is less energy-intensive than traditional insulation materials. Recycled denim insulation, made from post-consumer denim, offers superior thermal performance as well as soundproofing benefits. It's free of harmful chemicals and allergens, contributing to healthier indoor air quality.
Sources
1.https://www.elematic.com/learn-precast/what-is-precast-concrete/sustainability-in-precast/
2.https://www.startus-insights.com/innovators-guide/top-10-construction-industry-trends-innovations-in-2021/
3.https://www.bigrentz.com/blog/construction-technology
4.https://www.bigrentz.com/blog/construction-technology
5.https://buildingrenewable.com/10-environmental-benefits-of-recycled-steel/
6.https://www.mdpi.com/2071-1050/16/6/2347
7.https://www.builderspace.com/sips-construction-24-pros-and-cons
8.https://www.sips.org/blog/redefining-sustainable-construction-with-structural-insulated-panels-sips