- Home
- Support and Downloads
- Info Center
- Cordless FAQs
Hilti cordless tools FAQs
Find answers to frequently asked questions about Hilti cordless power tools and batteries
Read on to discover everything you need to know about cordless tools and batteries.
Can't find the answer to your question? Get in touch with us below!
CORDLESS PLATFORMS
What is the difference between the 12V, 22V, 36V and Nuron cordless platform?
Nuron is the latest addition to the Hilti cordless portfolio, bringing our current 22V & 36V tools onto the same batteries. It provides you with a single high-performing battery platform for all your Hilti cordless tools. With Nuron, you can reduce complexity from your business because you can carry out all your applications – from screwdriving to concrete cutting – using the same set of high-performing interchangeable 22V Nuron batteries and chargers. And because the platform is connected, you also get access to a range of data-driven services designed to simplify equipment management.
NURON
How exactly do the smart connectivity features of Nuron work?
Nuron tools generate data which is then stored on the attached battery. When the battery is charged, the data is transmitted securely via cellular networks to the cloud. There is no interruption to your workflows because no special setup, configuration or other action is required. The data from Nuron can provide you with proactive services that help reduce downtime (such as battery replacement alerts). The data also gives transparency on the tool's last charged location and usage and provides you with actionable insights to help you make more informed decisions about your tool park. These data-driven services are available using the ON!Track platform which is available via the app and web.
Are all the connectivity features of Nuron available to all customers?
All Nuron customers have access to the platform's onboard battery diagnostics and to tool management features via the ON!Track mobile app. You can use the app to scan tools and batteries, access videos and instructions, find related products (like accessories) or easily submit repair orders. When a battery is no longer performing at optimal levels, you can also perform a quick and easy exchange directly from the app. If you are a Hilti Fleet Management and ON!Track tool park management customer, you’ll also benefit from a growing portfolio of premium data-driven services and software.
All chargers delivered with our Fleet Management programme come connected as standard. This means you’ll be informed of any potential issues with batteries immediately. You’ll also be able to locate tools quickly or identify tools that are sitting idle so you can get them out to your teams. You can also use the data that is securely collected by the Nuron platform to identify and analyse usage trends. Use this information to help build a tool park that really works for your business.
Do I need a lot of training to use the connected Nuron platform?
No. The Nuron platform has been designed for easy use without interrupting your workflows. Our dedicated customer support team are ready to answer any questions you might have and help you make use of your data.
Will Nuron track anything like working hours, worker productivity or other sensitive data?
No. The data generated by the Nuron platform is not linked to individual users. It is only machine information - such as details about when and how tools are being used, error codes, charging location or battery status. If you want to link tool data and user information, you can do this voluntarily using relevant functions from our ON!Track digital equipment management solution. Contact us for more information about the connectivity of our new battery platform.
UPGRADING TO NURON
Do I have to change to Nuron or can I keep using the Hilti cordless tools I already have?
You can continue using the Hilti cordless tools you have. However, we highly recommend an upgrade to Nuron because the platform delivers higher performance and greater connectivity benefits at a similar price.
Are Nuron tools more expensive than existing 22V and 36V Hilti tools?
The Nuron platform is similarly priced to our other cordless platforms. For more details on specific tools, visit the product pages on our website, contact our customer support team, speak to your account manager or visit one of our Hilti stores.
What about spare parts and accessories? Do I need to replace all these too?
No – not all spare parts and tool accessories need to be replaced. For more information, visit the product pages on our website, contact our customer support team, speak to your account manager or visit one of our Hilti stores.
How long will existing 22V and 36V Hilti tools be available?
The current 22V and 36V platforms will continue to be supported and available for as long as necessary.
Can I still use the 12V platform with sub-compact tools for lighter-duty tasks?
Yes. You can continue using Hilti 12V battery power tools for lighter-duty applications in hard-to-reach corners and we will continue to develop this platform.
Can I use the 22V and 36V Hilti tools I already have with Nuron batteries?
You can use an adapter to run almost all of your existing 22V tools with Nuron batteries. Check the product pages on our website, contact customer support or visit a Hilti store for details on whether the adapter can be used with specific tools. Unfortunately, there is no adapter for 36V tools.
BATTERIES
How should I store and handle lithium-ion batteries?
For longer battery life, higher productivity and increased protection for your teams, we recommend the following:
- Storage temperature of between –20°C and +40°C
- Use the built-in State-of-Health check of your Nuron batteries to ensure they are fully productive
- Do not store batteries on the charger. Always remove the battery from the charger when charging is completed
- Never store batteries where they are exposed to direct sunlight, on heat sources or behind glass
- Ambient operating temperature of between -17°C and +60°C
- Regularly inspect battery packs and avoid charging or discharging if damage is visible
- Keep batteries clean – remove dust and debris with a dry soft brush or a dry rag
- Do not use batteries for other purposes (e.g. as hammers)
What does battery state of health mean?
Battery state of health refers to the remaining life of lithium-ion battery packs. All lithium-ion batteries lose capacity and performance as they age – whether it's tool batteries or laptop and mobile phone batteries. With the Nuron platform, the state of health function gives you guidance on when a battery pack should be replaced. This helps you make sure you are always working with the most productive tools possible.
Do lithium-ion batteries work in colder weather?
The ambient operating temperature should be between -17°C and +60°C, while the optimal range is from 10°C to 30°C. Batteries cannot be charged below 0°C.
Should lithium-ion batteries be fully discharged before charging?
No, you do not need to fully discharge a lithium-ion battery before charging. Li-ion batteries are very versatile and there are no specific concerns about battery life being shortened because of "memory effects" from partial charging and discharging.
How long do Hilti lithium-ion batteries last?
Nuron batteries contain high-quality lithium-ion cells that are designed to deliver high performance and long life. Individual battery life depends on a number of factors such as what sort of tool is being used, user force, frequency of use, and ambient temperature, among others.
ENVIRONMENTAL SUSTAINABILITY
How can I safely dispose of lithium-ion batteries?
We take responsibility for our products throughout their lifetime and at the end of life, so that they don’t end up in landfill sites. You can dispose of your Hilti batteries at a Hilti store, or consult with your local governmental rubbish disposal or public health and safety resources for disposal instructions. Before disposing of your batteries, please cover the contacts with non-conductive material (for example, electrical tape). Do not dispose of batteries as household waste.
Can Hilti cordless tools be recycled?
Please dispose of your Hilti tools at a Hilti store and we will ensure it's correctly reused and/or recycled. If possible, we use the spare parts from the tools we collect - otherwise we recycle the materials in it. Our tools have high proportions of steel, copper and aluminum and over 70% of the tool’s mass can be recycled for a variety of purposes. We are also continually working to raise this percentage.
What does Hilti do to reduce the environmental impact of its power tools?
At Hilti, we look at the entire lifecycle of our products. For example, we currently use 23% recycled material on average in our products (against a global average of 8%), while 100% of our production runs on renewable energy. We also focus on tool repairs rather than replacement and when a tool reaches end of life, we collect it for free with our global collection partners. Anything that cannot be reused is recycled with our audited 3rd party logistics partners. This ensures that we can assess tools for reuse, either as full tools for donations or as components for our spare parts reuse programme. Since our tools are over 70% metal, most of the tool's weight can re-enter international commodity markets. For more information, visit the sustainability section of our website.
What does Hilti do to reduce the environmental impact of its lithium-ion batteries?
Batteries collected by our global network of reverse logistics are recycled by 3rd party partners who specialise in the field of battery recycling. They extract specific materials including cobalt, nickel and lithium. These materials are then reused in future manufacturing processes. We are working with recycling partners to improve the recycling process to ensure that as much of these more valuable materials are extracted as possible.
More Questions?
If you have a question we've not been able to answer, we'd love to hear from you! Get in touch with our team below.